Aug 4, 2017 |  Sustainability


3 Unique Industries Finding Creative Uses for Solar Energy


At 27 million degrees Fahrenheit, the sun produces large amounts of energy. This energy can be collected through a solar device that converts sunlight into electricity. Solar energy is reliable and easy to use, making it attractive to numerous businesses. In 2017, switching to solar is a trend that's gaining momentum in unexpected places. More and more unlikely industries are integrating solar energy into their everyday operations because of its cost effectiveness and reliability. 

Solar installations are projected to increase by two million in the U.S. by 2018 and four million by 2022. With a focus on reducing carbon footprints and increasing energy savings, uncommon businesses are deciding to go green.

Here’s how three industries are taking advantage of solar opportunities and transforming the way they do business.

Winning the Battle Against High Costs

The U.S. military is harnessing the sun’s power by implementing solar energy on the battle field. Remotely-stationed troops lack resources and need access to off-grid power. This need has led to increased solar energy use in the field. In fact, military branches utilize a variety of solar equipment, including solar panels, solar tent shields, and solar cell batteries.  This equipment does not require fuel resupply, which could put military personnel at risk. Another advantage is its light weight, allowing for easy portability and less restrictiveness for troops.

Renewable energy is expected to continue growing, with the Navy, Army, and Air Force focusing on plans to expand the use of solar energy. Twenty-five percent of the energy consumed in military facilities is expected to be sourced from renewable energy by 2025, resulting in billions of dollars being saved over time. At the U.S. Air Force Academy located in Colorado Springs, a 6-megawatt solar system was installed to produce electricity for the facility. This led to savings of more than $650,000 per year.

The shift to solar offers the military many benefits such as reduced costs, decreased dependency on fossils fuels, and protection against security issues.

Teamwork Makes Solar Work

Sports teams across the United States are using solar to power stadiums and arenas. Fans attend some of the largest sporting events in facilities functioning solely with energy from the sun. Approximately 70,000 fans watched Super Bowl LI in a stadium operated by solar canopy structures and solar panels. Along with that facility, Indianapolis Motor Speedway in Speedway, Indiana, has one of the largest solar systems among U.S. sports complexes.

Solar energy is a sensible choice for the sports industry. The switch helps reduce environmental damage and decreases risks associated with climate change. These benefits have led to 25 stadiums, arenas and raceways located in 12 states to invest in solar equipment. Thanks to these installations, facilities reduced the use of nearly 22,000 metric tons of carbon dioxide.  

Earning Extra Credit From the Sun

Bright futures aren’t just for students these days – thanks to the help of the sun, schools across the country are transitioning to solar power. A school building’s flat rooftop design enables easy installation of solar photovoltaic cells or solar thermal systems. Utilizing solar power in schools helps protect the environment, reduces water usage, and provides teachers with unique teaching opportunities.

One major advantage is decreased costs. A report by The Solar Foundation found that if 450 school districts installed a solar PV system, they could save $1,000,000 over thirty years. Because of the potential savings, many schools are eager to benefit from the sun’s natural power.

Making the Case for Solar Across Industries

Some of the world’s largest industries are operating efficiently thanks to solar energy. In fact, falling solar costs make this energy source more accessible now than ever before. These decreased costs also mean major benefits for businesses. Some of these include reduced operating costs, a reliable energy source, reduced consumption of fuels, and tax incentives. From small to large organizations, industries are being transformed by the sun’s power.

New Call-to-action

 


Stay Informed With Wesco


STAY INFORMED

  • © 2016 WESCO International, Inc. All rights reserved.