Lighting the Way to Mine Safety

For the mining industry, safety and lighting go hand in hand. Navigating harsh and hazardous conditions requires a well-lit work area. Slip and fall accidents are the second-leading cause of non-fatal mining-related injuries according to a report by the National Institute for Occupational Safety and Health (NIOSH).


Mining Safety: Reduce Arc Flash Exposure Economically

For electrical workers, there’s no danger more worrying than an arc flash. Non-contact electrical burns from an arc flash are the biggest cause of electrical injuries in the mining industry. But as dangerous as an arc flash is for mining personnel, companies face further concerns such as lost man-hours, lawsuits, fines, equipment damage and facility downtime. Reducing the risk of an arc flash doesn’t require a complete facility overhaul or redesign. By updating and refurbishing existing equipment, you can create a safer environment economically.  


Drilling Down on the Right Cable for Mining Industry Trends

Just from looking at an open-pit mine, it’s easy to see that mining requires a significant capital investment. Between expensive equipment and a specialized workforce, players in the mining game know that keeping maintenance costs under control is paramount. This year, we’ve seen several trends emerging in the international mining industry. The first step in staying competitive is knowing these trends. The next step is having cost-effective equipment that keeps your mine running.


 
 
  • © 2016 WESCO International, Inc. All rights reserved.