Thursday, May 19, will mark the official grand opening of our new branch in Sacramento, Calif. To honor the occasion, we’re hosting an open house from 3-7 p.m. PDT featuring a supplier trade show, interactive product demonstrations, and a casino-themed atmosphere.
While the branch officially opened for business in March 2015, we’re excited to give the rest of the public a chance to see the 55,000-square-foot facility. But if the venue itself isn’t enticing enough, here are three more reasons that will make this event worth attending.

The Entertainment
Sure, it’s all about business at the end of the day, but why not do it with flair? This event will up the fun factor – casino style. With the help of Sacramento-based Casino Party 2U, we’re giving attendees an opportunity to bond over games of Craps, Texas Hold’em, Three Card Draw, and Black Jack using chips they earn from vendors.
The Food
Delicious food can make almost any event more appealing. Citchy Co., whose food truck was voted #1 in Sacramento, will serve a variety of gourmet sandwiches, fries and drinks at the event. Check out their menu to see why our mouths are watering already.
The Camaraderie
Our open houses attract suppliers and customers from all types of industries. This event will be a prime opportunity to network with other businesses and potentially set up new partnerships. And once the business talk is done, unwind with your new peers with some beer and wine courtesy of Primo Bar.